S32 design studio installtion

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 design studio installtion

1,785 Views
gopichakrala
Contributor I

Hi NXP team,

I tried to install S32 design studio, but it is not installing.

it shows that it installed properly but it is not installed.

find the attached log files.

Thank you in advance for you help.

Regards,

Gopi

Labels (1)
Tags (1)
1 Reply

1,601 Views
martin_kovar
NXP Employee
NXP Employee

Hello Gopi,

according the log it looks like the installation was canceled by user.

Check Disk Space:         C:\NXP\S32DS__v1.3
                          Status: SUCCESSFUL
                          Additional Notes: NOTE - Required Disk Space: 2,069,747,198; Free Disk Space: 19,215,368,192


INSTALLATION WAS CANCELLED BY USER DURING PRE-INSTALLATION

S32DS version 1.3 is not recommended to use anymore. Could you please try to download newest version (2018.R1) and try to install this, instead of 1.3?

Regards,

Martin