S32 Design Studio for S32 Platform Version: 3.4 Build id: 201217 (Update 3)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Studio for S32 Platform Version: 3.4 Build id: 201217 (Update 3)

1,901件の閲覧回数
Can_Do_bus
Contributor III

I have installed S32 Design Studio for S32 Platform
Version: 3.4
Build id: 201217 (Update 3)

 

On Ubuntu 20.04 without any issues.

 

However it doesn't come with S32SDK_S32K1XX_RTM_4.0.2, how can I manually install it? Only freemaster SDK is installed.

 

I have the S32 Design Studio ARM - that comes with S32SDK V 3.0.0

 

Can you suggest how the S32SDK can be installed on the design studio on Linux with code examples

0 件の賞賛
返信
1 返信

1,863件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

unfortunately S32K1xx SDK is not supported on Linux host machine. 

 

Jiri 

0 件の賞賛
返信