S32 Design Studio for Power v3.4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Studio for Power v3.4

2,070件の閲覧回数
xuan
Contributor I

hello

When I call the static link library file (.a) created by myself, there is an error when compiling. I would like to ask the cause of this error. And how to solve it?

xuan_0-1672989875579.pngxuan_1-1672989924210.png

 

0 件の賞賛
返信
3 返答(返信)

2,058件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi,

please make sure the compiler options for library and app match.

Stan

0 件の賞賛
返信

2,046件の閲覧回数
xuan
Contributor I

hi

I make sure the library and the application's compiler options match.

xuan_0-1673241404539.png

xuan_1-1673241454982.png

 

 

0 件の賞賛
返信

2,040件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello,

The compiler options @stanish was referring to would be found in the 'Standard S32DS C Compiler' section of the Tool Settings menu (visible in the 2nd image you shared on the start of this thread).

Best Regards,

Mike

0 件の賞賛
返信