S32 Design Studio for ARM license expiring in 13 days,how can i solve it?Thanks!
S32 Design Studio for ARM
ActivationId: F625-BD17-9FB6-009D
Evaluation Days: 13
Feature Version: 2.2
Feature Status: Evaluation (13 days)
解決済! 解決策の投稿を見る。
I have returned your license, when you re-activate, the new expiration date will be loaded.
Best Regards,
Mike
Hi Mike,
I made the KEA8 firmware using S32 Design Studio for ARM v2.2 3 year free license.
The current project is over.
We are currently selling products with firmware (*.srec) created by the project.
When the license expires, will I be unable to sell products made with the current firmware?
Best Regards,
romeo
Hello Romeo,
I believe you are confusing the Software License Agreement with the Software Tools License.
The Software License Agreement covers how the software you develop using the NXP provided SDKs may be used and distributed. The terms and conditions you agreed to when you installed the SDK specify the limitations. I'm not aware there is a defined time limit, but you should review this agreement to ensure you understand the limitations and that you are in compliance.
The Software Tool License for S32 Design Studio is what enables you to activate and make use of the IDE for development purposes. You cannot use the IDE without an active license. This license is generally provided with expiration of 3 years, however, we can extend the tool license for you at any time.
I hope this answers your question.
Best Regards,
Mike
Sorry, I have the same issue for
S32 Design Studio for ARM v2018 R1
Activation code: E281-F80C-438F-6887
Please, could you renew also it.
Thanks
Hello,
This one has been renewed through 2025. Please re-activate your installation.
Best Regards,
Mike
Hi NXP-Team,
my license has expired too. Can you please help me with that?
Best regards,
Markus
Hello Markus,
I have extended your entitlement through 2025. Please re-activate your installation.
Best Regards,
Mike
Hi, I have the same issue:
Fulfillment ID: 153510107
Expiration Date: Aug 1, 2022
Product: S32 Design Studio for ARM v2018 R1
Machine: 70990A1E3F1FE8C48BAD3BAF14F6163E9DA45CDC
Activation Code: CE54-8A45-DFCB-2A14
Hi Jonas,
I have extended your entitlement. Since your license has already expired, you probably won't be able to refresh. You will need to re-activate using the existing activation code. It should prompt you when you launch S32 Design Studio.
Best Regards,
Mike
Hi my license is expired too. Can you extend it? thank you!
S32 Design Studio for PA E200 v2.0
4A7F-2866-9BBB-431E
It needs NXP Employee to extend.
Hello,
Your license was extended through 2025.
Please refresh or reactivate your license.
Best Regards,
Mike
Same problem here, license expired, cant renew the license.
ActivationID: D70F-D40C-4AD2-DF97
Version 2018.R1
Can somebody help me with this?
Hello Artur,
I have extended your entitlement through 2025. Please refresh the license from within the Help->NXP Licenses menu. Or you might have to return and re-activate using same activation code as before.
Please let me know of any further issue.
Best Regards,
Mike
Hi,
I would like my license extended as well.
License Applicable to Product(s):
| Version | Description | ||
| 2018 | S32 Design Studio for ARM v2018 R1 |
| 1 |
| 194470497 |
| Jun 4, 2022 |
| S32 Design Studio for ARM v2018 R1 |
Activation Code:
| CCF8-7C0D-1FEF-C281 |
Hi,
I extended your license till end of 2025. Please enter your activation code in S32DS again.
Jiri
Hi Mike,
Kindly renew
Fulfillment ID: | 192400897 |
Expiration Date: | Mar 15, 2022 |
Product: | S32 Design Studio for ARM v2018 R1 |
Machine: | 6DB8562794A476A701EEF087DCDA7006DDF50E2C |
Activation Code: | 89AE-671C-7A13-D4D3 |
Hello,
Your entitlement has been extended through 2025. Please either 'refresh' the license from the NXP Licenses menu (Help -> NXP Licenses) or re-activate using the code you shared.
Best Regards,
Mike
Hi Mike,
My S32 Design Studio for Power architecture license expired (B86D-B7D4-0C1D-3021), can you please extend it?.
Hi Ramesh,
I have extended your entitlement through 2025. Please refresh the license or reactivate your install.
Best Regards,
Mike
Hello
I have the same problem too.
Can you reactivate my license for S32 Design Studio for ARM V1.3, please?
Activation ID: 816A-E5D9-CA6E-E65E