S32 Design Studio and Keil Ulink2 support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Studio and Keil Ulink2 support

2,552件の閲覧回数
StefanoGattazzo
NXP Employee
NXP Employee

Hi everyone,

Is it possible to use Keil ULINK2 as programmer/debugger for S32 Design Studio (S32K144)? 

If not is it something we consider or this must be considered by Keil?

Thanks and BR

Stefano

タグ(3)
0 件の賞賛
返信
2 返答(返信)

2,308件の閲覧回数
robertboys
Contributor IV

Hello

NXP OpenSDA is Arm CMSIS-DAP compliant.

So is a Keil ULINK2, ULINK-ME and ULINKplus.

I think it would be worth a try.

Bob

0 件の賞賛
返信

2,308件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello Stefano,

I  checked reference manual for S32DS for ARM and only following debuggers are officially supported:

P&E Multilink/Cyclone/OpenSDA (with PnE GDB Server)
SEGGER J-Link (with SEGGER GDB Server)

iSystem, Lauterbach, and IAR debuggers support by S32DS Application Project and S32DS Library Project
wizards

So, from my point of view, Keil debugger will not work.

Regards,

Martin

0 件の賞賛
返信