Hello,
I am using NXP S32K3X4 with PE Micro Debugger (Multilink Universal) and while debugging I am getting the Runtime Error 216 at 0348A5D6 in S32Design Studio
any idea regarding this?
Hi @V_ishal
On the board that you are seeing the "Runtime Error", can you please do the following:
Then try again and see if it resolves the issue?
This power-up procedure manage that SBC starts with the disabled watchdog. Four orange LEDs indicate active 12, 5, 3.3 and 1.5 V power supply domains.
Hi @juan_see
Tried these steps multiple time but still issue is not resolved.
It's not flashing/debugging on that particular board, I am attaching some stepwise snapshots kindly have a look at it
Hi V_ishal
I am also currently facing the same issue.
My board is also experiencing runtime errors 216 and is not reconnecting after disconnecting.
Therefore, I am currently testing other functions using a different board. The runtime error occurred while adding MCAL-Sbc_fs26.
I would like to know if the issue has been resolved.