RAppID [MPC5744P]

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RAppID [MPC5744P]

1,605 Views
abdelrhman
Contributor III

Manually, I downloaded rbf file into the dev board. then I used RAppID BL to program an application code. The RAppID erased the flash and downloaded the application code successfully as shown in the figure below. However, the application code doesn't work.
Are there any steps missing to download an application code successfully ????

abdelrhman_0-1657809050565.png

 

0 Kudos
Reply
1 Reply

1,600 Views
mikedoidge
NXP Employee
NXP Employee

Hello @abdelrhman ,

Please ensure you have setup your application properly so that the RCHW value, address of KEY, etc are set at proper addresses and values, etc.

Device

Communication supported

Device tested

RBF file

Boot-loader areas

CAN

(500Kb/s)

UART

(115200b/s)

rchw

m_text

MPC5744P

CAN0

(PB0-PB1)

UART2

(PF14-PF15)

MPC5744P-FML09 1N15P

MPC5744P-FMLQ8 0N65H

PPG5744P-FMMM8 0N65H

MPC5744P.rbf

0x00F98000 - 0x00F98004

0x00F98008 - 0x00F9FFFF

v  RCHW and KEY used in the application

Please refer to section 5.2 for defining the value of RCHW and KEY

Please refer to section 6.2 for setting up the application project with S32DS tool

v  Notes

The MPC574xP RBF boot-loader occupies 16K memory blocks starting at 0x00F98000. Please note that the address of the final position in “.srec” file will depend on the device memory map

The user application is allowed on RAM from the base address + 0x1400 to the end of RAM

How to use RCHW and KEY in the application

Before starting the application, the boot-loader will search for RCHW and KEY value in the application. If found, the boot-loader will consider the application suitable and run it. Otherwise, the boot-loader will not run the application and stay in waiting mode.

  • RCHW: the value of this variable will be programmed into the first 4 bytes of the application.

The only value for RCHW is 0x005A0000

  • The KEY value is set at the last position of the application.

The only value for KEY is 0x55AA55AA

Project setup on S32 Design Studio

  • Open S32DS for Power Architecture
  • Create a new default project wizard

image.png
Figure 6.2.1

  • Change the “flashchw.c” file by adding the following piece of code:

#if defined(START_FROM_FLASH)

#include "typedefs.h"

#define MPC57xx_ID 0x005A0000 /* RCHW boot ID for MPC57xx devices */

#define VLE_ENABLE 0x01000000 /* VLE is enabled */

#define CPU2_ENABLED 0x00000001

#define CPU0_ENABLED 0x00000002

#define CPU1_ENABLED 0x00000008

extern void _start(void);

extern void _startcore1(void);

extern void _startcore2(void);

#define TARGET_CORES (CPU0_ENABLED | CPU1_ENABLED | CPU2_ENABLED)

//#define RCHW_VAL (MPC57xx_ID | TARGET_CORES)

#define RCHW_VAL 0x005A0000

const volatile uint32_t APPKEY __attribute__ ((section(".appkey"))) = 0x55AA55AA;

const uint32_t __attribute__ ((section(".rchw"))) RCHW [] = {

                                                                        RCHW_VAL,

            /* cpu0_reset_vector */ (uint32_t)_start,

            /* delay */                                            0x2DC6C0,                                          // 3 sec

            /* application key */ (uint32_t)&APPKEY,

            /* cpu2_reset_vector */ (uint32_t)_startcore2,

            /* cpu1_reset_vector */ (uint32_t)_startcore1};

#endif /* defined(START_FROM_FLASH) */

  • Modify the linker file as shown below by adding a new line *(.appKey) into the .text segment:

image.png

Figure 6.2.2

 

  • The example output .srec file generated by the compiler integrated in S32 Design Studio:
  • The first part of the file:

image.png

Figure 6.2.3

  • The last part of the file:

image.png

Figure 6.2.4

 

Hope it helps,

Mike

0 Kudos
Reply