Project with S32 Design Studio and IAR program flash issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Project with S32 Design Studio and IAR program flash issue

4,254件の閲覧回数
chaitanya_kalyani
Contributor III

Hello,

I am facing issue for flash and debug the program when created with IAR compiler. 

Following below steps

1. New Application project 

chaitanya_kalya_0-1599542291332.png

and when I compile it then It don't have any issue.

But when I try to flash it then it is just building and after some time PE multilink is getting disconnected. 

chaitanya_kalya_1-1599542441094.png

after abort getting below error 

chaitanya_kalya_2-1599542469477.png

Please help me to solve this problem.

thank you in advance.

0 件の賞賛
返信
6 返答(返信)

4,234件の閲覧回数
chaitanya_kalyani
Contributor III

Hello @jiri_kral 

 

Thank you for quick response. I am using S32K144 EVB and board is powered up properly. When I flash example project then there is no issues. Issue is only when I create new project and try to flash it. 

 

I am attaching sample project that I have created.

0 件の賞賛
返信

4,244件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

What is your board - it is custom one or NXP EVB? Is your board properly powered up? Is tour PE Multilink probe correctly connected to board? 

 

Jiri 

0 件の賞賛
返信

4,239件の閲覧回数
chaitanya_kalyani
Contributor III

I am using S32K144 EVB. Board is powered up properly. When I use example project then there is no issues. Issue is only when I create new project. 

0 件の賞賛
返信

4,226件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

I tried import your project and there is no issue with flashing on my side. I used PE Micro Multilink FX. Can  you share output from Debug console - if there is any? You can also try to re-install PE Micro drivers - with default install path located in c:\NXP\S32DS_ARM_v2.2\Drivers\ 

 

Jiri

0 件の賞賛
返信

4,204件の閲覧回数
chaitanya_kalyani
Contributor III

Hello @jiri_kral ,

 

Thank you for the quick response.

 

For flash might be there is some issue with the EVB board. It is not able to flash with PE Multilink but able to flash with OpenSDA. 

 

 

0 件の賞賛
返信

4,197件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

 

what about power supply when connected to PE Micro Multilink? Did you provide external 12V or you are using USB? 

 

Jiri

0 件の賞賛
返信