Problem with Debugger S32DS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with Debugger S32DS

ソリューションへジャンプ
34,455件の閲覧回数
koehlerl
Contributor IV

Hi,

I want to debug in a function, but then I get this error from the debugger. See  attachment.

What is the problem ?

Br

Lutz

ラベル(1)
1 解決策
33,385件の閲覧回数
koehlerl
Contributor IV

Hi,

I have updated the SEGGER J-Link GDB Server to V6.33d(beta) and the JLinkARM.dll to V6.33d.

Now it seems to work well.

BR Lutz

Von: [email protected]

Gesendet: Dienstag, 26. Juni 2018 19:50

An: Köhler, Lutz <[email protected]>

Betreff: Re: - Re: Problem with Debugger S32DS

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: Problem with Debugger S32DS

reply from Jiri Kral<https://community.nxp.com/people/[email protected]?et=watches.email.thread> in S32 Design Studio - View the full discussion<https://community.nxp.com/message/1028508?commentID=1028508&et=watches.email.thread#comment-1028508>

元の投稿で解決策を見る

11 返答(返信)
33,384件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

Are you able step in the function or the message appears right after you hit F5 (or click on step in) ? Can you please share your project? 

It is also possible that you are performing for example flash erase in flash target program ( means that program erases itself). What about RAM target, it is working? Also make sure that EEPROM is partitioned properly before you are using it. 

Jiri

0 件の賞賛
返信
33,384件の閲覧回数
koehlerl
Contributor IV

Hi,

the message appears right after I launch the debugger.

I can flash the program. It works fine.

It is only a problem with the debugger.

Sorry but I can’t chare the project.

Lutz

Von: [email protected]

Gesendet: Montag, 25. Juni 2018 11:22

An: Köhler, Lutz <[email protected]>

Betreff: Re: - Re: Problem with Debugger S32DS

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: Problem with Debugger S32DS

reply from Jiri Kral<https://community.nxp.com/people/[email protected]?et=watches.email.thread> in S32 Design Studio - View the full discussion<https://community.nxp.com/message/1027787?commentID=1027787&et=watches.email.thread#comment-1027787>

0 件の賞賛
返信
33,384件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

You can try to modify Segger debug settings - like speed and so on. Do you have another debugger available - for example PE Micro? 

Anyway, I never saw this kind of error before. Without project it is hard to say what may be wrong. 

Jiri

0 件の賞賛
返信
33,383件の閲覧回数
koehlerl
Contributor IV

Hi,

I haven’t any other debug probe.

I changed the settings from the segger debug probe, but this doesn’t help.

I only have the problem, since the project is bigger and has more code.

text data bss dec hex

113088 7612 15400 136100 213a4

Lutz

Von: [email protected]

Gesendet: Montag, 25. Juni 2018 12:01

An: Köhler, Lutz <[email protected]>

Betreff: Re: - Re: Problem with Debugger S32DS

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: Problem with Debugger S32DS

reply from Jiri Kral<https://community.nxp.com/people/[email protected]?et=watches.email.thread> in S32 Design Studio - View the full discussion<https://community.nxp.com/message/1027790?commentID=1027790&et=watches.email.thread#comment-1027790>

0 件の賞賛
返信
33,383件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

okay - I'll try to create similar scenario with similar size and let you know if I can reproduce the issue. Did you try find answer on Segger forum? 
SEGGER - Forum 

Jiri

0 件の賞賛
返信
33,381件の閲覧回数
koehlerl
Contributor IV

Hi,

on Segger forum I didn‘t found any answer for the problem.

I found nothing to issue S322DS with segger j-link prob.

Lutz

Von: [email protected]

Gesendet: Montag, 25. Juni 2018 14:13

An: Köhler, Lutz <[email protected]>

Betreff: Re: - Re: Problem with Debugger S32DS

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: Problem with Debugger S32DS

reply from Jiri Kral<https://community.nxp.com/people/[email protected]?et=watches.email.thread> in S32 Design Studio - View the full discussion<https://community.nxp.com/message/1027841?commentID=1027841&et=watches.email.thread#comment-1027841>

0 件の賞賛
返信
33,381件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Can you please share at least elf file? You can send it to my email [email protected]. With current info - I can't help you. 

Jiri

0 件の賞賛
返信
33,386件の閲覧回数
koehlerl
Contributor IV

Hi,

I have updated the SEGGER J-Link GDB Server to V6.33d(beta) and the JLinkARM.dll to V6.33d.

Now it seems to work well.

BR Lutz

Von: [email protected]

Gesendet: Dienstag, 26. Juni 2018 19:50

An: Köhler, Lutz <[email protected]>

Betreff: Re: - Re: Problem with Debugger S32DS

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: Problem with Debugger S32DS

reply from Jiri Kral<https://community.nxp.com/people/[email protected]?et=watches.email.thread> in S32 Design Studio - View the full discussion<https://community.nxp.com/message/1028508?commentID=1028508&et=watches.email.thread#comment-1028508>

33,381件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi Lutz, 

I have similar scenario:

text             data          bss          dec             hex filename
113128       8192         15592     136912         MTRDEVKSPNK144_S32DS.elf

Full segger debug console output:

SEGGER J-Link GDB Server V6.22e Command Line Version

JLinkARM.dll V6.22e (DLL compiled Jan 8 2018 11:44:25)

Command line: -if swd -device S32K144 -endian little -speed 1000 -port 2331 -swoport 2332 -telnetport 2333 -vd -ir -localhostonly 1 -singlerun -strict -timeout 0 -nogui
-----GDB Server start settings-----
GDBInit file: none
GDB Server Listening port: 2331
SWO raw output listening port: 2332
Terminal I/O port: 2333
Accept remote connection: localhost only
Generate logfile: off
Verify download: on
Init regs on start: on
Silent mode: off
Single run mode: on
Target connection timeout: 0 ms
------J-Link related settings------
J-Link Host interface: USB
J-Link script: none
J-Link settings file: none
------Target related settings------
Target device: S32K144
Target interface: SWD
Target interface speed: 1000kHz
Target endian: little

Connecting to J-Link...
J-Link is connected.
Firmware: J-Link Lite-Cortex-M V8 compiled Sep 15 2016 12:05:01
Hardware: V8.00
S/N: 398000830
OEM: IAR
Checking target voltage...
Target voltage: 4.98 V
Listening on TCP/IP port 2331
Connecting to target...Connected to target
Waiting for GDB connection...Connected to 127.0.0.1
Reading all registers
Read 4 bytes @ address 0x00000000 (Data = 0x20007000)
Received monitor command: speed 1000
Target interface speed set to 1000 kHz
Received monitor command: clrbp
Received monitor command: reset
Resetting target
Received monitor command: halt
Halting target CPU...
...Target halted (PC = 0x00000410)
Received monitor command: regs
R0 = 00000000, R1 = 00000000, R2 = 00000000, R3 = 00000000
R4 = 00000000, R5 = 00000000, R6 = 00000000, R7 = 00000000
R8 = 00000000, R9 = 00000000, R10= 00000000, R11= 00000000
R12= 00000000, R13= 20007000, MSP= 20007000, PSP= 00000000
R14(LR) = FFFFFFFF, R15(PC) = 00000410
XPSR 01000000, APSR 00000000, EPSR 01000000, IPSR 00000000
CFBP 00000000, CONTROL 00, FAULTMASK 00, BASEPRI 00, PRIMASK 00
Reading all registers
Read 4 bytes @ address 0x00000410 (Data = 0x490BB672)
Received monitor command: speed auto
Select auto target interface speed (2000 kHz)
Received monitor command: flash breakpoints 1
Flash breakpoints enabled
Received monitor command: semihosting enable
Semi-hosting enabled (Handle on BKPT)
Received monitor command: semihosting IOClient 1
Semihosting I/O set to TELNET Client
Received monitor command: SWO DisableTarget 0xFFFFFFFF
SWO disabled successfully.
Received monitor command: SWO EnableTarget 0 0 0x1 0
ERROR: Failed to measure CPU clock frequency: second loop count is less than first one! (176<=10618)

Failed to enable SWO. Could not measure target CPU frequency.
Read 4 bytes @ address 0x00000410 (Data = 0x490BB672)
Received monitor command: clrbp
Received monitor command: reset
Resetting target
Received monitor command: halt
Halting target CPU...
...Target halted (PC = 0x00000410)
Downloading 1024 bytes @ address 0x00000000 - Verified OK
Downloading 16 bytes @ address 0x00000400 - Verified OK
Downloading 4096 bytes @ address 0x00000410 - Verified OK
Downloading 4096 bytes @ address 0x00001410 - Verified OK
Downloading 4096 bytes @ address 0x00002410 - Verified OK
Downloading 4096 bytes @ address 0x00003410 - Verified OK
Downloading 4096 bytes @ address 0x00004410 - Verified OK
Downloading 4096 bytes @ address 0x00005410 - Verified OK
Downloading 4096 bytes @ address 0x00006410 - Verified OK
Downloading 4096 bytes @ address 0x00007410 - Verified OK
Downloading 4096 bytes @ address 0x00008410 - Verified OK
Downloading 4096 bytes @ address 0x00009410 - Verified OK
Downloading 4096 bytes @ address 0x0000A410 - Verified OK
Downloading 4096 bytes @ address 0x0000B410 - Verified OK
Downloading 4096 bytes @ address 0x0000C410 - Verified OK
Downloading 4096 bytes @ address 0x0000D410 - Verified OK
Downloading 4096 bytes @ address 0x0000E410 - Verified OK
Downloading 4096 bytes @ address 0x0000F410 - Verified OK
Downloading 4096 bytes @ address 0x00010410 - Verified OK
Downloading 4096 bytes @ address 0x00011410 - Verified OK
Downloading 4096 bytes @ address 0x00012410 - Verified OK
Downloading 4096 bytes @ address 0x00013410 - Verified OK
Downloading 4096 bytes @ address 0x00014410 - Verified OK
Downloading 4096 bytes @ address 0x00015410 - Verified OK
Downloading 4096 bytes @ address 0x00016410 - Verified OK
Downloading 4096 bytes @ address 0x00017410 - Verified OK
Downloading 4096 bytes @ address 0x00018410 - Verified OK
Downloading 4096 bytes @ address 0x00019410 - Verified OK
Downloading 4096 bytes @ address 0x0001A410 - Verified OK
Downloading 1488 bytes @ address 0x0001B410 - Verified OK
Downloading 8 bytes @ address 0x0001B9E0 - Verified OK
Downloading 4096 bytes @ address 0x0001B9E8 - Verified OK
Downloading 4096 bytes @ address 0x0001C9E8 - Verified OK
Read 4 bytes @ address 0x00000410 (Data = 0x490BB672)
Read 2 bytes @ address 0x00004486 (Data = 0xF001)
Read 2 bytes @ address 0x00004486 (Data = 0xF001)
Read 2 bytes @ address 0x00004486 (Data = 0xF001)
Received monitor command: regs
Comparing flash [....................] Done.
Erasing flash [....................] Done.
Programming flash [....................] Done.
Verifying flash [....................] Done.
R0 = 00000000, R1 = 00000000, R2 = 00000000, R3 = 00000000
R4 = 00000000, R5 = 00000000, R6 = 00000000, R7 = 00000000
R8 = 00000000, R9 = 00000000, R10= 00000000, R11= 00000000
R12= 00000000, R13= 20007000, MSP= 20007000, PSP= 00000000
R14(LR) = FFFFFFFF, R15(PC) = 00000410
XPSR 01000000, APSR 00000000, EPSR 01000000, IPSR 00000000
CFBP 00000000, CONTROL 00, FAULTMASK 00, BASEPRI 00, PRIMASK 00
Reading all registers
Read 4 bytes @ address 0x00000410 (Data = 0x490BB672)
Setting breakpoint @ address 0x00004486, Size = 2, BPHandle = 0x0001
Starting target CPU...
...Breakpoint reached @ address 0x00004486
Reading all registers
Read 4 bytes @ address 0x00004486 (Data = 0xFFF9F001)
Removing breakpoint @ address 0x00004486, Size = 2
Reading 64 bytes @ address 0x00004480
Reading 64 bytes @ address 0x000044C0
Read 4 bytes @ address 0x20006FFC (Data = 0x0000043D)
Read 4 bytes @ address 0x20006FFC (Data = 0x0000043D)
Read 4 bytes @ address 0x0000043C (Data = 0x0000E7FE)
Read 4 bytes @ address 0x20006FFC (Data = 0x0000043D)
Read 2 bytes @ address 0x00000410 (Data = 0xB672)
Read 2 bytes @ address 0x00000412 (Data = 0x490B)
Read 4 bytes @ address 0x00000442 (Data = 0x70000000)
Read 2 bytes @ address 0x00000414 (Data = 0x4A0A)
Read 4 bytes @ address 0x00000440 (Data = 0x00000000)
Read 2 bytes @ address 0x00000416 (Data = 0x4B0A)
Read 4 bytes @ address 0x00000442 (Data = 0x70000000)
Read 2 bytes @ address 0x00000418 (Data = 0x4C09)
Read 4 bytes @ address 0x00000440 (Data = 0x00000000)
Read 2 bytes @ address 0x0000041A (Data = 0x4D09)
Read 4 bytes @ address 0x00000442 (Data = 0x70000000)
Read 2 bytes @ address 0x0000041C (Data = 0x4E08)
Read 4 bytes @ address 0x00000440 (Data = 0x00000000)
Read 2 bytes @ address 0x0000041E (Data = 0x4F08)
Read 4 bytes @ address 0x00000442 (Data = 0x70000000)
Read 2 bytes @ address 0x00000420 (Data = 0x46B8)
Read 2 bytes @ address 0x00000422 (Data = 0x46B9)
Read 2 bytes @ address 0x00000424 (Data = 0x46BA)
Read 2 bytes @ address 0x00000426 (Data = 0x46BB)
Read 2 bytes @ address 0x00000428 (Data = 0x46BC)
Read 2 bytes @ address 0x0000042A (Data = 0x4806)
Read 4 bytes @ address 0x00000446 (Data = 0x2A212000)
Read 2 bytes @ address 0x0000042C (Data = 0x4685)
Read 2 bytes @ address 0x0000042E (Data = 0x4806)
Read 4 bytes @ address 0x0000044A (Data = 0x29110001)
Read 2 bytes @ address 0x00000430 (Data = 0x4780)
Read 4 bytes @ address 0x20006FF4 (Data = 0x00000100)
Read 1 bytes @ address 0x20006FF2 (Data = 0xFF)
Read 1 bytes @ address 0x20006FF3 (Data = 0x1F)
Read 4 bytes @ address 0x20006FF4 (Data = 0x00000100)
Read 1 bytes @ address 0x20006FF2 (Data = 0xFF)
Read 1 bytes @ address 0x20006FF3 (Data = 0x1F)

So, I can't reproduce your issue. 

actually - the issue looks related to segger plugin/firmware/connection. I found this thread - [SOLVED] Remote failure reply ... - J-Link/Flasher related - SEGGER - Forum  

segger team recommends update firmware to version 6.32b. But mine is old one - 6.22e and works okay. 

Jiri

0 件の賞賛
返信
33,381件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello Lutz,

could you please specify your issue?

Which version of S32DS you use?

What is the project you debug?

What is the function and what is the body of the function which causes this problem?

What is the microcontroller you use?

What debug probe you use?

Could you please eventually share the project if it is not any one included in S32DS?

Regards,

Martin

33,379件の閲覧回数
koehlerl
Contributor IV

Hello,

I use S32DS Version 2018.R1

Debug probe is Segger J-link.

I can’t share the project.

I have the problem since my project has more code. I don’t think that is a problem with the function. I think it is a general problem with the code size.

Now I get this message. See debugger console.

It is not possible to debug.

Br Lutz

Von: b55689

Gesendet: Dienstag, 19. Juni 2018 14:46

An: Köhler, Lutz <[email protected]>

Betreff: Re: - Re: Problem with Debugger S32DS

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: Problem with Debugger S32DS

reply from Martin Kovar<https://community.nxp.com/people/b55689?et=watches.email.thread> in S32 Design Studio - View the full discussion<https://community.nxp.com/message/1025937?commentID=1025937&et=watches.email.thread#comment-1025937>

0 件の賞賛
返信