Problem in importing existing project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem in importing existing project

3,252 Views
nathan_
Contributor IV

I am using S32 Design Studio for power architecture. I created a project, but how can I open the 

project? it tells "some project cannot be imported because they already exist in the workspace"

How can i open the project?

0 Kudos
Reply
1 Reply

3,035 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

unfortunately, it is not possible to have two projects with the same name in workspace. So you have to rename the project or delete the project from the workspace.

Regards,

Martin

0 Kudos
Reply