P&E connection error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P&E connection error

2,753 Views
boyoungmun
Contributor I

Hi,

 

I use MPC574XG-324DS and MPC574XG-MB.

I tried to debug MPC5748G with P&E multilink universal FX using S32 Design Studio for power 1.1.

But an error occurred while connecting to the interface hardware.

 

I checked LED diode D1 was off and I added 250ms delay after reset in the debug configuration dialog.

But multilink was not connected. Would you please let me know how to connect hardware?

Labels (2)
0 Kudos
Reply
2 Replies

2,559 Views
stanish
NXP Employee
NXP Employee

Hello,

Could you please try to create a new project build it and debug?

Please make sure blue and yellow LEDs both lights on P&E pod. 

Could you try it with any other board if you have some.

Can you please attach the snapshot of the error you get (including details)?

Also the debugger log might help us to find the root cause.

To get the log please switch the console to GDB Traces (see below), copy and paste the log into a file and post it here.

pastedImage_1.png

Thank you!

Stan

0 Kudos
Reply

2,559 Views
boyoungmun
Contributor I

Dear Stan,

I tried to connect MCU and daughter card again, P&E error disaperaed.

Thank you for your support.

0 Kudos
Reply