Opensda PeMicro CDC Serial Port issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Opensda PeMicro CDC Serial Port issue

5,496件の閲覧回数
weisenzhang
Contributor I

hi, guys:

I can't access the serial port of opensda of s32k144 demo board, the seial driver can't be  installed correctly. 

here is my device and system information.My system is windows 7 64bit. thanks!

 

 

165488_165488.pngpastedImage_2.png

 

165487_165487.pngpastedImage_1.png

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

4,686件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi,

this looks like a driver issue.

Please check this blog: https://mcuoneclipse.com/2012/10/12/fixing-the-usb-drivers/ 

Stan

0 件の賞賛
返信

4,686件の閲覧回数
leekate-b45752
NXP Employee
NXP Employee

Hi Stanislav, 

The customer already did as followed as 'Fixing the USB Drivers | MCU on Eclipse ', but it kept being failed. 

Only CDC serial port error occurred, could you check the issue as below?

pastedImage_2.png

Best regards,

Kate Lee

0 件の賞賛
返信