Only CAN_0 in S32DS Debug view

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Only CAN_0 in S32DS Debug view

2,679 次查看
bdn
Contributor III

Hi,

 

why is there only CAN_0 in S32_Debug view as seen on the screenshot?

153614_153614.pngCAN.png

 

I'm using S32DS for PowerPC in verison 1.0 with MPC5748G Eval Board and 176QFP Daughtercard.

 

Regards,

Bernhard

标签 (2)
2 回复数

2,469 次查看
bdn
Contributor III

Hi,

this issue is _not_ fixed in S32 DS for Power Architecture 1.1.

Regards

2,469 次查看
martin_kovar
NXP Employee
NXP Employee

Hi Bernhard,

I checked the issue and you are correct, there is only CAN_0. It seems it is a bug, so I reported it immediately. Sorry for inconvenience, I hope it will be fix in the next release, which should be available at the end of June.

As a workaround, memory view could be used.

Regards,

Martin

0 项奖励
回复