Not able to figure out root of machine check exception

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Not able to figure out root of machine check exception

1,697 次查看
hiddenshadowny
Contributor I

I am using RRU SC667463  controller

I am facing machine exception , but looking at the stack frame from local and looking into the registers 

i am not able to figure out why it is exactly happening, it is very much random behavior 

pastedImage_1.png

I can see the Link register to be FFF0000, which shlould hold the return address but its illegal address.

Looking at MCSRR0 i can see FA3234 which is the content of the return address for isr

pastedImage_2.png

I am trying to figure out the exact reason behind the random exception but i am not able to map it correctly.

Regards,

Nishesh

标记 (3)
0 项奖励
回复
1 回复

1,611 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

it is possible share your project?

Jiri 

0 项奖励
回复