Need SW pkg - S32 RTD AUTOSAR 4.4 Version 3.0.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need SW pkg - S32 RTD AUTOSAR 4.4 Version 3.0.2

1,469 Views
randykrakora1
Contributor I

Looking to update my s32ds for generating configuration code for s32g, but when I try to install this package as an update, s32ds produces an error:

 

So I was told by an NXP FAE that I need to install the package by itself, but I cannot find it in my account. Apparently I need access to "Automotive SW -> S32G Standard Software", which I do not have yet in my account. Can I get this added to my account to find the package and install it?

 

Regards,

Randy Krakora

0 Kudos
Reply
1 Reply

1,433 Views
mikedoidge
NXP Employee
NXP Employee

Hi Randy,

The S32 RTD package has a prerequisite of the device development package. For you, that would be the 'S32G development package'. If you are connected to the web and your firewall isn't blocking, then you should be able to install this package directly from the update server using the 'Help -> S32DS Extensions and Updates'. You can actually install both the development package and the RTD package at the same time, the tool is smart enough to install them in the right order.

Let me know if you have further issues.

Mike

0 Kudos
Reply