Missing Std_Types.h

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Missing Std_Types.h

3,719件の閲覧回数
ArkAndyFraser
Contributor III

I have just upgraded to S32DS version 3.5 and have setup my pins and drivers.

I have generated the necessary files but when I try and compile I get the following error message:

Std_Types.h: No such file or directory

This file is included in one of the generated files Port_Ci_Port_Lp.h

/*==================================================================================================
*   Project              : RTD AUTOSAR 4.7
*   Platform             : CORTEXM
*   Peripheral           : PORT_CI
*   Dependencies         : none
*
*   Autosar Version      : 4.7.0
*   Autosar Revision     : ASR_REL_4_7_REV_0000
*   Autosar Conf.Variant :
*   SW Version           : 2.0.0
*   Build Version        : S32K1_RTD_2_0_0_D2308_ASR_REL_4_7_REV_0000_20230804
*
*   Copyright 2020-2023 NXP Semiconductors
*
*   NXP Confidential. This software is owned or controlled by NXP and may only be
*   used strictly in accordance with the applicable license terms. By expressly
*   accepting such terms or by downloading, installing, activating and/or otherwise
*   using the software, you are agreeing that you have read, and that you agree to
*   comply with and are bound by, such license terms. If you do not agree to be
*   bound by the applicable license terms, then you may not retain, install,
*   activate or otherwise use the software.
==================================================================================================*/

#ifndef PORT_CI_PORT_IP_H
#define PORT_CI_PORT_IP_H

/**
*   @file    Port_Ci_Port_Ip.h
*
*   @defgroup Port_IPL Port IPL
*   @{
*/

#if defined(__cplusplus)
extern "C" {
#endif

/*==================================================================================================
*                                          INCLUDE FILES
* 1) system and project includes
* 2) needed interfaces from external units
* 3) internal and external interfaces from this unit
==================================================================================================*/

#include "Std_Types.h"
#include "Port_Ci_Port_Ip_Cfg.h"
#include "Port_Ci_Port_Ip_Types.h"
#include "Port_Ci_Port_Ip_Defines.h"
#include "Devassert.h"

What am I doing wrong?

Version 3.5 feels like a massive backward step from 3.4 which was super easy to use

Andy

3 返答(返信)

2,744件の閲覧回数
mstroven
Contributor III

I've had to go back to DS3.4 with SDK RTM 4.0.2 to get something that mostly works as advertised.  However, the more I use the NXP SDK, the more I hate it...

2,972件の閲覧回数
Djuric
Contributor III

Any updates on this?

@ArkAndyFraserdid you manage to solve the problem with the missing Std_Types.h file being included in the generated RTD files?

I couldn't find  the Std_Types.h file even in the examples provided by NXP.

0 件の賞賛
返信

3,077件の閲覧回数
mstroven
Contributor III

3.6 Didn't improve things either.  These jokers don't bother to regression test.