What is the maximum clock freq for FTM of s32k144?
If it uses SPLL_CLK as a External clock for clock source.
and SPLL_CLK can be configured to 112MHz in HSRUN mode.
Is the Maximum clock freq for FTM 28Mhz ?
Because clock signal must not exceed 1/4 of FTM input clock which is 112Mhz in HSRUN mode.
Am I right?
If so, Are there any ways to boost up the FTM source clock?
Hi,
in my opinion - if you choose System Clock as clock source for FTM - the clock frequency for FTM depends on RUN mode. In HSRUN - the FTM clock is 112 MHz. Actually I didn't find any limitation related to 1/4 of system clock in Reference manual.
Jiri