MPC 5775B GPIO Interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC 5775B GPIO Interrupt

1,334 Views
DDosi
Contributor I

I want to get a user input from Push Buttons using interrupt on PIN PG3 to PG8 but there is no IRQ option to enable for these Pins.
Do MPC 5775 controller have only selected interrupt pins or i am doing something wrong.

Tags (2)
0 Kudos
Reply
1 Reply

1,329 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

In the past I made example code for these. You may download it here:

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5777C-SIUL-External-IRQ-GHS714/ta-p/1...

 

0 Kudos
Reply