J-Link GDB Server failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

J-Link GDB Server failed

10,152 Views
Anjalipurushothaman
Contributor III

Please find the attched error message getting while hitting Run configuration.

There are different J-link open SDA-Generic firmwares? which one needeed to be installed?

hardware- s32k3x8EVB-Q289

IDE - S32ds3.5

0 Kudos
Reply
4 Replies

10,141 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

it looks that you have PE Micro OpenSDA debug probe, not the J-Link one. You can fix it by create new debug configuration for PE Micro OpenSDA. 

0 Kudos
Reply

10,105 Views
Anjalipurushothaman
Contributor III
Inorder to create new configuration for PE Micro, that is not showing in the window(please refer the attached create,run configuration tab shared earlier).
0 Kudos
Reply

10,096 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

did you updated PE Micro package to latest version? 

jiri_kral_0-1687531457785.pngjiri_kral_0-1687531457785.png

 

 

 

0 Kudos
Reply

10,091 Views
Anjalipurushothaman
Contributor III
Yes, it is latest version. While using run configuration option (PE Micro debugger is not poping uo) wheras in the Debug tab it is showing.

Here I don't want to debug, I needto run the code into the target prcessor(Evaluation board)
0 Kudos
Reply