IntCtrl_Ip Driver - Settings not found

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IntCtrl_Ip Driver - Settings not found

1,455 Views
Riyasma07
Contributor III

Below is the screen shot of my system's S32DS for platform 3.5 settings.

Riyasma07_2-1702551309080.pngRiyasma07_2-1702551309080.png

One of my colleague's S32DS has the Generic Interrupt Settings tab was present. But in my S32DS that setting tab was not found.

Riyasma07_3-1702551511069.pngRiyasma07_3-1702551511069.png

Kindly help to resolve this issue.

0 Kudos
Reply
2 Replies

1,440 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Riyasma07 

I checked this in S32DS v3.4 and v3.5, and as it is shown in the below image, it looks like the new RTDs release Generic Interrupt Settings tab is no longer available.

VaneB_0-1702578661177.pngVaneB_0-1702578661177.png

 

B.R

VaneB

1,443 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

what's the target device and RTD version? 

0 Kudos
Reply