'Installing software' has encountered a problem.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

'Installing software' has encountered a problem.

4,678 Views
anvesh_tss
Contributor II

while am installing S32 Design Studio S32SDK_S32K14x_BETA_1.9.0 am getting the below errors as

"'Installing software' has encountered a problem"

"An error occurred while installing the items
session context was:(profile=SDKProfile, phase=org.eclipse.equinox.internal.p2.engine.phases.Install, operand=[R]com.nxp.s32ds.ext.ide.resources 1.0.0.201801241544 --> [R]com.nxp.s32ds.ext.ide.resources 1.0.0.201808141508, action=org.eclipse.equinox.internal.p2.touchpoint.eclipse.actions.InstallBundleAction).
The artifact file for osgi.bundle,com.nxp.s32ds.ext.ide.resources,1.0.0.201808141508 was not found."

Here is the attachment for what I selected in the updates to install and below to this the "Problem Occured"

sdk_prblm_1.PNGsdk_prblm_2.PNG

 

3 Replies

4,643 Views
anvesh_tss
Contributor II

Even Though i have insttalled 'S32 Design Studio S32K1XX Support Package', still getting the same issue.

0 Kudos
Reply

4,612 Views
mikedoidge
NXP Employee
NXP Employee

Hello @anvesh_tss,

From the error message it seems you are missing this package. The error message is indicating that it is a dependency.

mikedoidge_0-1677001021630.png

 

Please check the box to install this package as well. It should resolve your issue.

Best regards,

Mike

0 Kudos
Reply

4,657 Views
mikedoidge
NXP Employee
NXP Employee

Hello,

Probably this is due to missing the required dependency on the 'S32 Design Studio S32K1XX Support Package', where XX represents the digits of the specific S32K family device you intend to use.

Best Regards,

Mike