I integrated CCP driver, Reload the project into workspace but compiler errors occur.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I integrated CCP driver, Reload the project into workspace but compiler errors occur.

1,385 Views
ChenBowen
Contributor II

    I integrated CCP driver, and my project works well .  However,  I removed the project and  just reload the project into the workspace,  and so many compiler errors occur.....  I am using S32DS v2.1 with SDK 3.03. 

 CCP编译错误.PNG

0 Kudos
Reply
1 Reply

1,367 Views
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @ChenBowen , 

 

Please can you provide more information related to the issue. 

 

It may be because something going wrong with file inclusion, it seems it is including files multiple times. 

 

Please can you check the your code files are proper or not. Sometime it may give error for the not completing brackets. 

 

Please can you share the log for the current workspace : 

 

C:\Users\Public\[workspace_name]\.metadata

 

Thank you. Best regards. 

- Mehul Patel

0 Kudos
Reply