How to use S32K144 MCAL 4.0.3?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use S32K144 MCAL 4.0.3?

2,442 Views
hongjinzeng
Contributor IV

Hi everyone,

  This week I download the MCAL 4.0.3 with S32K144?Accroding to the MCAL_SampleApplication.pdf,I success to build the demo project.Then I download the file to the demo board with opensda.Now I want to know how to configurate the MCAL with the EB tresos?Do you have some user mannul about this?I need use Flash GPIO TRGMUX ADC WDOG Clock FlexCAN PDB FTM LPIT LPSPI SENT.

Thanks!

Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

1,980 Views
mikedoidge
NXP Employee
NXP Employee

Hello Hongjin Zeng,

Unfortunately, there is not much documentation on this. What I can suggest is that there is a SampleApplication with PDFs on how to use it included in the MCAL installation. It is the only tutorial to get started. It includes example of most modules like ADC, FlexCAN, etc. However, it assumes you already know how to use the tools.

I don’t have S32K14x MCAL installed, but the sample application is either in the root folder, or in a doc folder located in a similar location as for MPC574xG:

 

C:\NXP\AUTOSAR\MPC574XG_MCAL4_3_RTM_1_0_0\MPC574XG_MCAL4_3_RTM_1_0_0_Sample_Application\eclipse\plugins\IntegrationFramework_TS_T2D35M10I0R0\doc

Hope it helps,

Mike

0 Kudos
Reply