How to resolve building problem Errors:Field 'Bits' could not be resolved

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to resolve building problem Errors:Field 'Bits' could not be resolved

ソリューションへジャンプ
2,973件の閲覧回数
13761826501
Contributor III

Hi,

    I've encountered a building problem that not block the building process to link and generate *.elf file. 

    I really wanna know the root cause to it, really appreciately if someone can help me.

The problem caused by following step:

1. First I wrote a structure object like below:

13761826501_0-1663244143890.png

2. second , create a variable by using this structure and click build, 

3. build process work around and *.elf file generated, but "Problems" shows errors like below:

13761826501_1-1663244277585.png

13761826501_2-1663244297758.png

4. That's really confused me a lot, so I try to deleted all errors and try buiding project again. This time NO such errors occurred in "Problems".

13761826501_3-1663244429307.png

 

13761826501_4-1663244438940.png

5. But those errors  reappeared in "Problems" after I open the C source file which use the structure described in the first step

No proofs point out that the structure was wrong, but why those errors about "Field XXX could not be resolved" triggered while these errors would not block the build process? thank you !

0 件の賞賛
返信
1 解決策
2,940件の閲覧回数
13761826501
Contributor III

The target MCU is S32K146, Thank you also for presenting the reason for such a problem exist . Later I will check the update

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,941件の閲覧回数
13761826501
Contributor III

The target MCU is S32K146, Thank you also for presenting the reason for such a problem exist . Later I will check the update

0 件の賞賛
返信
2,959件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

what's your S32DS Version and target MCU? 

 

Earlier versions of S32DS has known issue - for some projects the build generates false positive errors. The errors was shown only in S32DS (S32DS is based on Eclipse) - but target was build successfully. In later S32DS version was this issue fixed. 

 

Jiri

0 件の賞賛
返信