How to install SDK S32K3 in S32DS Ver 3.5

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to install SDK S32K3 in S32DS Ver 3.5

Jump to solution
2,537 Views
dnewbe
Contributor III

I met problem install S32K3 SDK (SW32K3_S32DS_3.5_D2207) in S32DS version 3.5 when another PC.

Previously I installed S32DS version 3.4 and re-installed to version 3.5. So older PC is works on version 3.5 and SDK is SW32K3_S32DS_3.5_D2207.

I installed S32DS version 3.5 on new another PC but I failed install SDK to S32DS 3.5. S32DS is not connected SDK when I check in preference of my project.

So I un-installed S32DS 3.5 and I installed S32DS 3.4. but the error message is show "Software Activation Code is already used on this station for SW32_S32DS_3.5 apucOMPILER 2.0 when enter Activation Code.

I read other topic in this community about this kind installation and errors. But I can't solve my problem.

I'd like to use S32DS 3.5 and SW32K3_S32DS_3.5_D2207 SDK. Tell me how to clean previous information and how to re-install S32DS and SDK.

0 Kudos
Reply
1 Solution
2,440 Views
dnewbe
Contributor III

I resolved this issue.

The process of installing S32DS, installing update packages, and installing SDK brings a lot of confusion.
However, the problem has been resolved, but it is still confusing. Because the installation process that has been repeated so far is not that different.

Thanks.

View solution in original post

0 Kudos
Reply
3 Replies
2,520 Views
dnewbe
Contributor III

I tried more install again and I got success SD32DS version 3.5 and SW32K3_S32DS_3.5_D2207. But I don't understand why my re-install is works.

Anyway I got important point after install SD32DS.
1. need support package for SD32DS like as SW32K3_S32DS_3.5_D2207.
2. need RTD file like as SW32K3_RTD_4.4_2.0.1_DS_updatesite_D2207.
So I did two more install new software.

2,528 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Pay attention to following thread:

https://community.nxp.com/t5/S32-Design-Studio/S32-Design-Studio-for-S32-Platform-v-3-4-license-acti...

I believe it explains your issue.

0 Kudos
Reply
2,441 Views
dnewbe
Contributor III

I resolved this issue.

The process of installing S32DS, installing update packages, and installing SDK brings a lot of confusion.
However, the problem has been resolved, but it is still confusing. Because the installation process that has been repeated so far is not that different.

Thanks.

0 Kudos
Reply