How to install SDK S32K3 in S32DS Ver 3.5

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to install SDK S32K3 in S32DS Ver 3.5

跳至解决方案
5,240 次查看
dnewbe
Contributor III

I met problem install S32K3 SDK (SW32K3_S32DS_3.5_D2207) in S32DS version 3.5 when another PC.

Previously I installed S32DS version 3.4 and re-installed to version 3.5. So older PC is works on version 3.5 and SDK is SW32K3_S32DS_3.5_D2207.

I installed S32DS version 3.5 on new another PC but I failed install SDK to S32DS 3.5. S32DS is not connected SDK when I check in preference of my project.

So I un-installed S32DS 3.5 and I installed S32DS 3.4. but the error message is show "Software Activation Code is already used on this station for SW32_S32DS_3.5 apucOMPILER 2.0 when enter Activation Code.

I read other topic in this community about this kind installation and errors. But I can't solve my problem.

I'd like to use S32DS 3.5 and SW32K3_S32DS_3.5_D2207 SDK. Tell me how to clean previous information and how to re-install S32DS and SDK.

0 项奖励
回复
1 解答
5,143 次查看
dnewbe
Contributor III

I resolved this issue.

The process of installing S32DS, installing update packages, and installing SDK brings a lot of confusion.
However, the problem has been resolved, but it is still confusing. Because the installation process that has been repeated so far is not that different.

Thanks.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
5,223 次查看
dnewbe
Contributor III

I tried more install again and I got success SD32DS version 3.5 and SW32K3_S32DS_3.5_D2207. But I don't understand why my re-install is works.

Anyway I got important point after install SD32DS.
1. need support package for SD32DS like as SW32K3_S32DS_3.5_D2207.
2. need RTD file like as SW32K3_RTD_4.4_2.0.1_DS_updatesite_D2207.
So I did two more install new software.

5,231 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Pay attention to following thread:

https://community.nxp.com/t5/S32-Design-Studio/S32-Design-Studio-for-S32-Platform-v-3-4-license-acti...

I believe it explains your issue.

0 项奖励
回复
5,144 次查看
dnewbe
Contributor III

I resolved this issue.

The process of installing S32DS, installing update packages, and installing SDK brings a lot of confusion.
However, the problem has been resolved, but it is still confusing. Because the installation process that has been repeated so far is not that different.

Thanks.

0 项奖励
回复