I met problem install S32K3 SDK (SW32K3_S32DS_3.5_D2207) in S32DS version 3.5 when another PC.
Previously I installed S32DS version 3.4 and re-installed to version 3.5. So older PC is works on version 3.5 and SDK is SW32K3_S32DS_3.5_D2207.
I installed S32DS version 3.5 on new another PC but I failed install SDK to S32DS 3.5. S32DS is not connected SDK when I check in preference of my project.
So I un-installed S32DS 3.5 and I installed S32DS 3.4. but the error message is show "Software Activation Code is already used on this station for SW32_S32DS_3.5 apucOMPILER 2.0 when enter Activation Code.
I read other topic in this community about this kind installation and errors. But I can't solve my problem.
I'd like to use S32DS 3.5 and SW32K3_S32DS_3.5_D2207 SDK. Tell me how to clean previous information and how to re-install S32DS and SDK.
解決済! 解決策の投稿を見る。
I resolved this issue.
The process of installing S32DS, installing update packages, and installing SDK brings a lot of confusion.
However, the problem has been resolved, but it is still confusing. Because the installation process that has been repeated so far is not that different.
Thanks.
I tried more install again and I got success SD32DS version 3.5 and SW32K3_S32DS_3.5_D2207. But I don't understand why my re-install is works.
Anyway I got important point after install SD32DS.
1. need support package for SD32DS like as SW32K3_S32DS_3.5_D2207.
2. need RTD file like as SW32K3_RTD_4.4_2.0.1_DS_updatesite_D2207.
So I did two more install new software.
Pay attention to following thread:
I believe it explains your issue.
I resolved this issue.
The process of installing S32DS, installing update packages, and installing SDK brings a lot of confusion.
However, the problem has been resolved, but it is still confusing. Because the installation process that has been repeated so far is not that different.
Thanks.