How to generate bin, hex output files

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to generate bin, hex output files

11,613件の閲覧回数
leekate-b45752
NXP Employee
NXP Employee

Hello, 

How can I generate both of the bin and hex files at the same time after building?

I'm using S32DS for ARM v2.2.

Best regards,

Kate Lee

ラベル(2)
タグ(3)
0 件の賞賛
返信
5 返答(返信)

9,035件の閲覧回数
binZhang01
Contributor III

binZhang01_0-1717404782242.png

 

0 件の賞賛
返信

11,489件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi Kate, 

you can create .bin file by normal way in project settings and .hex file in post build steps in project properties: 
pastedImage_1.png

pastedImage_2.png

Jiri 

10,519件の閲覧回数
aiweixin
Contributor IV

Hi Jiri,

    I build the project to generate the bin and hex files according to your ways, but if failed.

    How can i do for it?

aiweixin_0-1667806021482.png

 

Best regards,

0 件の賞賛
返信

10,761件の閲覧回数
fxn
Contributor II

Hi Jiri,

Thanks for your reply.

0 件の賞賛
返信