How to extract range FFT values via UDP protocol?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to extract range FFT values via UDP protocol?

1,504件の閲覧回数
tasneemrahamank
Contributor I

Hello,

I am working on 77 GHz automotive radar and want to get some information on plotting the range FFT values. The microcontroller performs range fft on the received signals and transports the values to the host PC via UDP. Essentially, the data is located in the payload of the UDP packet and I want to retrieve the payload to a file on host PC which I am presuming should be complex double values. Is there any relevant information or some reference code I can get to plot these values in order to obtain range FFT? 

Thank you!

タグ(3)
0 件の賞賛
返信
0 返答(返信)