How do I enable Live View for variables in S32DS for power PC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do I enable Live View for variables in S32DS for power PC

2,216件の閲覧回数
NAIDU
Contributor III

Hi All,

  i want to view variable status in run time using S32DS with P&E universal for MPC5777C,i am not finding any option so please suggest how i can enable the this feature.

Thanks&Regards,

Naidu.

0 件の賞賛
返信
2 返答(返信)

2,021件の閲覧回数
stanish
NXP Employee
NXP Employee

Hello,

This question has been already answered here:

https://community.nxp.com/message/916979?commentID=916979#comment-916979 

Stan

0 件の賞賛
返信

2,021件の閲覧回数
NAIDU
Contributor III

Hi Stan,

   I seen this question but i am not finding suggested option in S32DS for power PC.In P&E blog,at the end it is mentioned that the “Real Time Expressions” view is not currently available for the E200 architecture, nor for Multi-Core debugging. Currently it is only available for Cortex-M devices such as NXP's Kinetis and LPC.

so is there any option to enable it.i think it need to be enabled by NXP?

Thanks&Regards,

Naidu

 

0 件の賞賛
返信