How can i setup the S32K without SDK in S32DS?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can i setup the S32K without SDK in S32DS?

2,339 Views
adrianwenger
Contributor III

I want to setup a project only with includedperipheral declarations from #S32K144.

How do i have to proceed?

Tags (2)
0 Kudos
Reply
3 Replies

2,128 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

I am not sure if I understand your question correct, but if you want to create project empty project for S32K144, click File->New->New S32DS project

pastedImage_1.png

Choose S32K144, insert project name and click next:

pastedImage_2.png

Do not change any settings on the following screen and click Finish

pastedImage_3.png

Regards,

Martin

0 Kudos
Reply

2,128 Views
adrianwenger
Contributor III

Hi Martin,

this Topic has already been resolved in the last week.

I don't know why it has apeared again as open...

Regards,

Adrian

0 Kudos
Reply

2,128 Views
martin_kovar
NXP Employee
NXP Employee

Hello Adrian,

I overlooked it. Maybe some database error. I am glad it was successfully resolved.

Regards,

Martin

0 Kudos
Reply