GHS compiler and S32 Design Studio for Arm 2018.R1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GHS compiler and S32 Design Studio for Arm 2018.R1

3,273件の閲覧回数
seonho_hong
Contributor I

hello,

now I'm trying to make a project with S32 Design Studio with below environment.

- MCU: S32k 146

-Compiler: Greenhils v2017.1.4

but I could not find the compiler setting on S32 Design Studio, only I could make a GCC project.

Do I need to install the plug-in for that? If yes, where can I find the material?

1 返信

2,526件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

please check this thread GHS plug-in can NOT successfully installed in S32DS for Power Architecture version 2017.R1 

You can contact Green Hills support to obtain toolchain plugin compatible with Eclipse Neon version (S32DS is based on Eclipse Neon). 

Hope it helps. 

Jiri