GCC/G++ Error for S32DS3.2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GCC/G++ Error for S32DS3.2

ソリューションへジャンプ
2,760件の閲覧回数
Alexander_Garcia
Contributor I

Hello,

I am seeing the errors in the attached screenshot. Do these matter if I plan on using an external compiler? 

Alexander_Garcia_0-1678817093662.png

Thanks,

Alex

 

ラベル(1)
0 件の賞賛
返信
1 解決策
2,741件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

I see, there should be no relation between generated code and the build toolchain. The code itself will be okay. 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,747件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi Alex, 

if you are going to use external compiler like IAR, you need to setup compiler - ideally in new project wizard. This method also configure paths and build variables. If you switch the compiler in an existing project - it sometimes brings such error messages and you need manually fix the paths and So on. 

 

0 件の賞賛
返信
2,745件の閲覧回数
Alexander_Garcia
Contributor I

Hey Jiri,

By external compiler, I meant to say that I'm exporting the emitted C files to a project somewhere else and using the compiler there. Would setting up the corresponding compiler in S32DS still be advantageous in this case?

0 件の賞賛
返信
2,742件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

I see, there should be no relation between generated code and the build toolchain. The code itself will be okay. 

0 件の賞賛
返信