Hello @ct5ctl,
This is all you need to change in the configuration tool and update the generated code:
Hello @ct5ctl,
Which S32K3 part do you have?
Do you use a certain RTD example or is it your custome code?
If it is your code, please share it so that we can test it on our side.
Is the HSE_FW enabled on the chip?
Regards,
Daniel
Hello @ct5ctl,
If you did not program the HSE_FW, it is not enabled, and we can exclude that.
Do you use an EVB or your own board?
Which RTD version do you use?
Can you update the letest one?
Thanks,
Daniel
The development board I use is S32K344_257BGA, as shown in the figure below
The RTD version I am using now is 2.0.1, I try to download and install the latest version of RTD (in the red frame), including mcal and sdk. But my s32ds can't recognize the latest version of RTD, what's the reason?
Hello @ct5ctl,
Thanks for providing the EVB version and the clock configuration.
The board has 40MHz crystal according the schematic of the S32K3-T-Box.
Can you change it in the configuration tool?
Thank you,
BR, Daniel
The chip package I had previously selected was 256 and now switched to the correct chip package 172.
The current situation is: every time I debug to Mcu_DistributePllClock(), it will get stuck, as shown in the figure below