Error when generating code for SCST Lib with S32K116, SDK 2.9.2 and IAR 8.22.2 c

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error when generating code for SCST Lib with S32K116, SDK 2.9.2 and IAR 8.22.2 c

1,995 Views
tminh
Contributor I

Hello,

S32DS failed to generate SCST Library code with SDK S32K1xx_BETA_2.9.2 and IAR 8.22.2 compiler with below Error:

Description:   

Generator: FAILURE: at line 86: Unknown macro: "PE_G_XLKR_COMPILER" (file: Drivers\S32K\S32K144_SDK01\SCST.drv)

Location: scst2

Type: Processor Expert Problem

I could generate SCST successfully when not using IAR compiler.

Please help me to clarify this issue.

Thanks and Regards,

Minh

0 Kudos
Reply
0 Replies