Error: While Installing S32_Design_Studio_3.5

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error: While Installing S32_Design_Studio_3.5

2,027件の閲覧回数
Ajay_R1
Contributor I

Hi,

I was trying to install S32_Design_studio_3.5.8 in my PC. After installation of design studio, I was trying install both S32k3XX development package & S32k3xx RTD Version 3.0.0. But for me in "S32 DS extension & update" section it was showing blank page.  Then i was trying to install through "updated zip package" from NXP website, While installing i'm getting some error.

For your reference, i have attached a image in below

Ajay_R1_0-1725425994033.png

 

Can someone please suggest a solution for this ? & Let me know if need more information

 

Regards,

Ajay_R1

 

0 件の賞賛
返信
4 返答(返信)

2,004件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Ajay_R1,

Please refer to HOWTO: offline install S32K3 RTD 3.0.0 in S32DS v3.5

If S32K3 RTD 3.0.0 still cannot be installed correctly, then I will forward this question to our S32DS experts.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

1,908件の閲覧回数
Ajay_R1
Contributor I

Hi @Robin_Shen,

As you suggested, I tried to download from offline packages, but still I'm facing same error. I have attached image in below.

Ajay_R1_0-1727086228349.png

Same problem we  are facing in many PC's. Because of that our project getting delayed.

So please let me know to solve this is issue. 

 

Regards ,

Ajay. R

 

 

0 件の賞賛
返信

1,895件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Did you follow the steps completely? Please tell me at which step you encountered this error?
If you followed any steps differently from me, please tell me.


If it still doesn't work, it is possible that your company firewall/network settings is blocking NXP repository site.

Have you tried to install it on your personal computer?

0 件の賞賛
返信

1,881件の閲覧回数
Ajay_R1
Contributor I

Hi

I have mentioned, step by step procedure  what I did while installing s32 design studio.

1st Step : Install S32 Design Studio 3.5 - There is no error.

2nd Step: Download and InstallS32 Design Studio 3.5 Update 2 D2302 - There is no error. 

3rd Step:  Download and Install S32 Design Studio 3.5.0 Development Package with support for S32K3xx devices - there is no error. But I was not able to see SDK's while creating new application project.

Then, I skipped 4th and 5th step Because I'm not going to use S32k396 & S32M276 RTD for development.

6th Step:  Download and install S32K3 Real-Time Drivers Version 3.0.0. - While doing this  step I  was facing some error. I have attached image in below.

Ajay_R1_0-1727112558809.png

These are the steps I did from my end. Please let me know, if i did any mistake. If it is correct then please let me know to solve this issues.

 

Regards

Ajay. R 

 

 

 

0 件の賞賛
返信