Develop with PE Multiink

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Develop with PE Multiink

ソリューションへジャンプ
2,301件の閲覧回数
fanziyu
Contributor IV

S9KEAZ128

SWD

PE Multilink

S32 Design Studio for ARM Version 2018.R1

Question1:I want to debug and program,how to configure the "Debug Configurations"?What is the difference among "Debug""Debug_Ram""Release"?

0 件の賞賛
返信
1 解決策
2,284件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello @fanziyu,

Please review the following thread:

What is the difference between Debug RAM and Debug Flash?

Generally, the most you need to do to configure the debug configuration is to setup the PEMicro Interface Settings on the Debugger tab. Select the type of PEMicro HW you are using (usually either USB Multilink or OpenSDA built into the evaluation board) and then the port you are using to connect to it from your PC.

If you don't already have a debug configuration for your project, then make sure you have your project selected in the Project Explorer before opening the Debug Configurations menu. This will allow the tool to automatically populate some fields with information from your project when you click 'New Launch Configuration'. Be sure to use the GDB PEMicro Interface Debugging section and not the GDB Hardware Debugging section in the panel on the left. Then 'Search Project...' for your executable on the Main tab (be sure to build your project so the executable is available). Switch to Debugger tab and 'Select Device', setup your PEMicro Interface Settings (make sure you have the device connected and powered up) and you are done. All other settings are defaulted to typical usage. Click 'Debug' to start debugging.

Best Regards,

Mike

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,285件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello @fanziyu,

Please review the following thread:

What is the difference between Debug RAM and Debug Flash?

Generally, the most you need to do to configure the debug configuration is to setup the PEMicro Interface Settings on the Debugger tab. Select the type of PEMicro HW you are using (usually either USB Multilink or OpenSDA built into the evaluation board) and then the port you are using to connect to it from your PC.

If you don't already have a debug configuration for your project, then make sure you have your project selected in the Project Explorer before opening the Debug Configurations menu. This will allow the tool to automatically populate some fields with information from your project when you click 'New Launch Configuration'. Be sure to use the GDB PEMicro Interface Debugging section and not the GDB Hardware Debugging section in the panel on the left. Then 'Search Project...' for your executable on the Main tab (be sure to build your project so the executable is available). Switch to Debugger tab and 'Select Device', setup your PEMicro Interface Settings (make sure you have the device connected and powered up) and you are done. All other settings are defaulted to typical usage. Click 'Debug' to start debugging.

Best Regards,

Mike

0 件の賞賛
返信