Debug Fail for empty device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debug Fail for empty device

2,332 Views
leekate-b45752
NXP Employee
NXP Employee

Hello, 

When the user try to debug with empty device(S32K144) and S32DS v2.2, but it was failed to reset.

Could you guide about the issue? 

leekate-b45752_1-1607921669471.jpeg

 

leekate-b45752_0-1607921634863.png

 

Best regards,

Kate Lee

0 Kudos
Reply
2 Replies

2,325 Views
jiri_kral
NXP Employee
NXP Employee

Hi Kate, 

 

um... interesting issue. Did you tried power cycle as suggested in output console? Also Emergency kinetis recovery may help. 

 

It is custom board or our EVB? 

 

BR, 

Jiri 

0 Kudos
Reply

2,312 Views
leekate-b45752
NXP Employee
NXP Employee

Hi Jiri, 

This issue was resolved by un-checked 'Use SWD protocol' box, but I couldn't understand the cause of the symptom. 

Best regards,

Kate Lee