Command-Line option

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Command-Line option

3,331 Views
malekben
Contributor II


Hi,

Is there a Command-Line option similaire to ppc_asm_to_vle of CodeWarrior that translates BookE assembler instruction to VLE instruction in C files.

 

Regards,

 

Malek.

Labels (2)
Tags (4)
0 Kudos
Reply
2 Replies

3,151 Views
stanish
NXP Employee
NXP Employee

Hello Malek,

There will be a new compiler option -Wa,-ppc_asm_to_vle in the coming release (v1.1) that enables translation (BOOKE -> VLE) for standalone assembler file only.

This version should be released by the end of May.

Regards,

Stan

0 Kudos
Reply

3,151 Views
martin_kovar
NXP Employee
NXP Employee

Hi Malek,

S32DS does not support translating BookE to VLE.

Regards,

Martin

0 Kudos
Reply