Command-Line option

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Command-Line option

3,338件の閲覧回数
malekben
Contributor II


Hi,

Is there a Command-Line option similaire to ppc_asm_to_vle of CodeWarrior that translates BookE assembler instruction to VLE instruction in C files.

 

Regards,

 

Malek.

ラベル(2)
タグ(4)
0 件の賞賛
返信
2 返答(返信)

3,158件の閲覧回数
stanish
NXP Employee
NXP Employee

Hello Malek,

There will be a new compiler option -Wa,-ppc_asm_to_vle in the coming release (v1.1) that enables translation (BOOKE -> VLE) for standalone assembler file only.

This version should be released by the end of May.

Regards,

Stan

0 件の賞賛
返信

3,158件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hi Malek,

S32DS does not support translating BookE to VLE.

Regards,

Martin

0 件の賞賛
返信