Codewarrior project to S32 Design studio

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior project to S32 Design studio

4,686 Views
maximillion
Contributor II

Hi,

I want to open Code Warrior project in S32 Design Studio. It is possible? If it yes how can I do

thanks

0 Kudos
Reply
7 Replies

4,671 Views
maximillion
Contributor II

Thanks for answering

Also, here is my second situation.

I have to open Code Warrior project in Kinetis Design Studio 3 IDE. Could you share with me AN about this topic?

0 Kudos
Reply

4,651 Views
Robin_Shen
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

4,640 Views
maximillion
Contributor II

maximillion_0-1637837430787.png

Firstly thanks for quick answer.

 I try to import Code Warrior Project which is complied GCC complier but I have an error. 

GCC complier properly for kinetis design isn't it? I thought yes this error still exist.

How can I fix that? Could you give me tricks about this topic.

Tags (1)
0 Kudos
Reply

4,609 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Did you click Convert CodeWarrior project file...?

Convert CodeWarrior project file....png

0 Kudos
Reply

4,598 Views
maximillion
Contributor II

Ekran Alıntısı.PNG

Yes I clicked after that I included LIN_Stack libraries.

But I have error and warrnings. Code warrior used to FLASH for debug. Maybe this is problem?

I use to your recommended document actually step by step but cant still convert. Where is the problem?

 

 

0 Kudos
Reply

4,543 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Sorry I am not familiar with this part, I suggest submitting this question to CodeWarrior for MCU.

0 Kudos
Reply

4,679 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

I recommend you to read: AN5282 CodeWarrior to S32 Design Studio (S32DS) Migration Guide
Hope it helps.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply