Checking if you already have SW32_S32DS_3.4 license

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Checking if you already have SW32_S32DS_3.4 license

6,454件の閲覧回数
nxf47333
NXP Employee
NXP Employee

Hi,

I un-installed S32DSV3.4 and Install again, but install stuck at Checking if you already have SW32_S32DS_3.4 license

 

0 件の賞賛
返信
21 返答(返信)

5,730件の閲覧回数
manju9401
Contributor II

manju9401_0-1651829491378.png

I have tried deleting rm -rf /usr/local/share/macrovision/storage/FLEXnet/


Still the installation is stuck and not proceeding further

0 件の賞賛
返信

5,717件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello Manjunath,

Did you install all of the Linux libraries listed in the installation guide?

What version of Linux are you using?

Best Regards,

Mike

0 件の賞賛
返信

5,688件の閲覧回数
manju9401
Contributor II

Yes, I have installed all the dependencies.

I am using Ubuntu 20.04

0 件の賞賛
返信

5,675件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello Manju,

The S32 Design Studio does not support Ubuntu 20.04. The most recent version supported is 18.04. Later this year, we plan to release a new version which will support a newer version of Ubuntu. Until then, you are on your own to make this work, we cannot support it.

Best Regards,

Mike

0 件の賞賛
返信

5,798件の閲覧回数
thosewhowish2b
Contributor II

Hello,

I have the same problem, installer gets stuck at licensing, @ 6% progress.

Sudo does not help. Running within a terminal or not makes no difference. Sometimes it asks for sudo password, sometimes it asks for the activation code.

I'm on an Ubuntu 21.10. I had been using S32DS on an Ubuntu 20.04 thus far, without much problem.

Can someone take another look at this? I'd be glad to collect logs or whatever, just tell me what to do.

Best regards,

0 件の賞賛
返信

5,773件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello Wesley,

The S32 Design Studio v3.4 supports Ubuntu versions 16.04 and 18.04. This is stated within the release notes. In the upcoming release, we will add support for 20.04. We cannot support use of versions outside of those listed in the release notes. Some customers report issues using 20.04, if you had it working, you were ahead of the game. Our advice, go back to what you had working.

Best Regards,

Mike

0 件の賞賛
返信

6,355件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello Alvin,

You could try to re-initialize the trusted storage:

Windows host:

-> Delete 'C:\ProgramData\FLEXNet'

This folder may be hidden by default, so then it would be necessary to change Windows Explorer settings to show hidden items.

Linux host:

/usr/local/share/macrovision/storage

Are you installing to Windows or Linux host?

Best regards,

Mike

0 件の賞賛
返信

6,347件の閲覧回数
nxf47333
NXP Employee
NXP Employee

Hi,

my PC is windows hot, per your suggestion, i deleted  C:\ProgramData\FLEXNet, and try to install again,

but issue is same, installing stuck at Checking if you already have SW32_S32DS_3.4 license

0 件の賞賛
返信

6,321件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello Alvin,

Is the user account used to login to Windows a member of the administrators group?

Could you provide the installation log file?
C:\NXP\S32DS.3.4\_S32 Design Studio for S32 Platform 3.4_installation\Logs

Best regards,

Mike

0 件の賞賛
返信

6,288件の閲覧回数
nxf47333
NXP Employee
NXP Employee

Yes.

No Log file, only JRE folder,

if I ended Java(TM) Platform SE binary(2), Software Activation Code window will be pop out. it's very confuse.

TKS

0 件の賞賛
返信

6,278件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello Alvin,

This seems to be some Java version conflict. You might try to remove or rename from User Environment Variables, Variable: TMP, Value:C:\Users\{username}\AppData\Local\Temp folder and try the install again. If installation is completed successfully, then return the C:\Users\{username}\AppData\Local\Temp variable to original state.

Best regards,

Mike

0 件の賞賛
返信

6,262件の閲覧回数
nxf47333
NXP Employee
NXP Employee

Per you suggestion, i tried, but issue is same.

0 件の賞賛
返信

5,216件の閲覧回数
sto
NXP Employee
NXP Employee

Hi,

did you find a solution for this?

Having the same problem (using Windows 10); none of the suggestions in this thread helped.

Best Regards,

Sebastian

0 件の賞賛
返信

4,964件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello Sebastian,

Could you check the following folder for a log file and share it?

C:\NXP\S32DS.3.4\_S32 Design Studio for S32 Platform 3.4_installation\Logs

Best Regards,

Mike

0 件の賞賛
返信

4,931件の閲覧回数
luyu
Contributor I

Hello

     Actually there is no log file in the folder as other people meet the same issue.

    

0 件の賞賛
返信

4,919件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello @luyu 

Could you please share the exact error message you are receiving? A screen capture is enough.

It could be an issue related to the version of the FlexNet Publisher included in the installer. Please go to https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/Troubleshooting-Activation-fails-with-... and try the solution for error message #2. After this it may let you complete the install. Also, try to enable 'Windows 7 compatibility mode' before executing the installer EXE.

Best Regards,

Mike

0 件の賞賛
返信

5,212件の閲覧回数
manju9401
Contributor II

Removed all of the design studio related files, then it got installed.

 

Try to remove each and every file related to design studio and then install. It works fine

 

4,913件の閲覧回数
luyu
Contributor I

Hello

I've met the same issue as you do. And  I’ve already deleted the files in the C:NXP and the C:Program data: FlexData. I don’t know which files needed to be deleted.

Could you share the experience about which files needed to be deleted?

0 件の賞賛
返信

4,893件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello @luyu 

Please check my reply from yesterday. I do not see your error message.

Best Regards,

Mike

0 件の賞賛
返信

4,983件の閲覧回数
luyu
Contributor I

Hello

       I‘m meeting the same issue as you do.

       But I don't know how to find all the related files with design studio

0 件の賞賛
返信