Can't build projects after upgrading S32 Design Studio

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't build projects after upgrading S32 Design Studio

Jump to solution
3,240 Views
ArkAndyFraser
Contributor III

I have just upgraded S32 Design Studio from 3.4 to 3.5 and now none of my projects build.

All I get is the following error:

ArkAndyFraser_0-1702135542544.png

What am I missing?

Andy

Tags (1)
0 Kudos
Reply
1 Solution
3,117 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Yes, and in the future, only the S32K1 RTD version will be updated and the SDK version will no longer be updated.

View solution in original post

0 Kudos
Reply
6 Replies
3,187 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Andy,

According to the currently available information, we don’t have any plan to integrate S32SDK S32K1XX 4.0.3 into S32DS 3.5 or above version. So please install S32SDK S32K1xx RTM 4.0.3 in S32 Design Studio 3.4.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
3,155 Views
ArkAndyFraser
Contributor III

Robin,

Thanks for your reply.

So, are you saying that I cannot update S32 Design Studio beyond version 3.4?

I am using the FS32K144 device.

Andy

0 Kudos
Reply
3,143 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Yes. If you use S32K1 SDK RTM 4.0.x, please do not update S32DS v3.4 to v3.5. If you want to use S32K1 RTD 2.0.0 or higher, please install S32DS v3.5.

0 Kudos
Reply
3,134 Views
ArkAndyFraser
Contributor III

Thanks Robin,

So, going forward, if I want to keep my S32 Design Studio up to date with the latest version, I should be installing RTD instead of SDK ?

Andy

0 Kudos
Reply
3,118 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Yes, and in the future, only the S32K1 RTD version will be updated and the SDK version will no longer be updated.

0 Kudos
Reply
3,111 Views
ArkAndyFraser
Contributor III

Robin,

Okay, that is all good to know

Thanks for all your help.

Andy

0 Kudos
Reply