About Fatal error[Li001]: could not open file error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About Fatal error[Li001]: could not open file error

3,165件の閲覧回数
Hoon
Contributor III

Hi

I am using IAR workbench. Now when i compiled my project code, below error message occured.

Fatal error[Li001]: could not open file "D:\SVN\Model\trunk\project\App_IAR\Debug" (failed opening file: 액세스가 거부되었습니다.)

Where to find this file and how I can fix this?

In addition, I received the setting environment from co-worker, but I'm the only one having a problem.

IDE : S32 Design Studio for ARM Version 2.2 / MCU : S32K144

0 件の賞賛
返信
1 返信

3,124件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

please check if you have write permission in D:\SVN\Model\trunk\project\App_IAR\Debug folder. It looks, that S3DS is not able write output files there. Also create new workspace may fix the issue. 

 

Jiri

0 件の賞賛
返信