|
|
|
| Product Release Announcement Automotive Processing S32 Design Studio for ARM 2.2 | |
|
|
|
January 31, 2020 |
The Automotive Processing's Embedded Tools Team at NXP Semiconductors is pleased to announce the release of the S32 Design Studio for Arm® v2.2. Here are some of its major features:
NOTE Support for S32V234 was moved to S32 Design Studio for S32 Platform 3.x and not included into S32 Design Studio for ARM anymore. The complete S32 Design Studio for ARM 2.2 release notes are attached below. Installation NotesPlease visit the S32 Design Studio for ARM product page - download section or direct link to download the installer. The installer requires the NEW Activation ID to be entered during the installation. You should receive an email that includes your Activation ID after starting the download.
Technical Support S32 Design Studio issues are tracked through the S32 Design Studio Public NXP Community space: https://community.nxp.com/community/s32/s32dsS32 Design Studio
|
|
Hi Mike,
I'm a bit confused.
W.
Hello Q_man,
Thank you for pointing out the error in the date. This was a copy/paste error. I have now corrected it.
As for the versioning, I apologize for this, we know it is confusing. We expect the current format to remain for now as it is standardized for NXP.
Best Regards,
Mike
The installer does not seem to accept a console installation method
My OS is Ubuntu 20.04 running the Java virtual machine as recommended by the Release Notes. The GUI installation kept hanging on the splash, when the progress bar was very near the end. This is why I tried console mode
The following is an output from my shell
family@family-desktop:~/Downloads$ ./S32DS_ARM_Linux_v2.2.bin -i console
Preparing to install
Extracting the installation resources from the installer archive...
Configuring the installer for this system's environment...
Launching installer...
=======================================================
Installer User Interface Mode Not Supported
The installer cannot run in this UI mode. To specify the interface mode, use the -i command-line option, followed by the UI mode identifier. The valid UI modes identifiers are GUI, Console, and Silent.
=======================================================
I have also tried the switch -i Console too
Is there any other way of installing the software?
Hello adam.hamilton@seeingmachines.com,
We have tried a similar scenario on our end. We used fresh Ubuntu 20.04LTS image, then Update/Upgrade and then followed the steps in the Installation guide for Linux host. Everything works out of box.
Could you please check if an installation log file was created? Perhaps it would contain some clue. Look for a .log file in: \NXP\S32DS_ARM_v2.2\_S32 Design Studio for ARM Version 2.2_installation\Logs\
Best Regards,
Mike