xgate access violation details - not available?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

xgate access violation details - not available?

2,488件の閲覧回数
Xbot
Contributor II
hi all,
 
I had a query on xgate memory protection and tried to ask a technical support from freescale. from what i understood from the reply i got, there seem to be no way of determining the details of the errors (address of error, cause...) when the xgate causes an access violation interrupt.
 
i am designing a function that checks for faults inside the system and i need to know the details of the errors i receive. this details are used for diagnostics.
 
is this how s12x is designed? can somebody explain?
 
 
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,487件の閲覧回数
Steve
NXP Employee
NXP Employee
xbot there is detailed XGATE debugging information in AN3458 and AN3555.


Message Edited by Steve on 2008-04-21 09:08 AM
0 件の賞賛
返信

1,487件の閲覧回数
Xbot
Contributor II
thanks. an3555 is very useful.
0 件の賞賛
返信