xgate access violation details - not available?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

xgate access violation details - not available?

2,481 次查看
Xbot
Contributor II
hi all,
 
I had a query on xgate memory protection and tried to ask a technical support from freescale. from what i understood from the reply i got, there seem to be no way of determining the details of the errors (address of error, cause...) when the xgate causes an access violation interrupt.
 
i am designing a function that checks for faults inside the system and i need to know the details of the errors i receive. this details are used for diagnostics.
 
is this how s12x is designed? can somebody explain?
 
 
标签 (1)
0 项奖励
回复
2 回复数

1,480 次查看
Steve
NXP Employee
NXP Employee
xbot there is detailed XGATE debugging information in AN3458 and AN3555.


Message Edited by Steve on 2008-04-21 09:08 AM
0 项奖励
回复

1,480 次查看
Xbot
Contributor II
thanks. an3555 is very useful.
0 项奖励
回复