win64 driver for ASP12 board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

win64 driver for ASP12 board

1,143 次查看
maximzaharov
Contributor I

ASP12 board with NI Elvis-2.

CodeWarrior S12 5.1 installed, but not consist drivers for Windows-64bit (on Windows 7 32 bit good working, but on Windows 7 or 8 64 bit - no ("unknown device")).

Drivers on www.pemicro.com also only for Windows-32. Were can i get driver, or it not exist?

Sorry my english.

标签 (1)
0 项奖励
回复
1 回复

1,067 次查看
Martin35804
NXP Employee
NXP Employee

hi,

first try to contact PEmicro for the avialable drivers:

http://www.pemicro.com/support/

Then you could consider to use the virtual machine to run the 32bit application and drivers.

https://www.virtualbox.org/wiki/Downloads

Then you could try a little workaround regarding the 64bit system. If you have the 32bit installed folder try to copy it as it is to a 64bit machine.

I hope this will work.

0 项奖励
回复