using array declared in "C" code in assembly for S12X

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

using array declared in "C" code in assembly for S12X

4,755件の閲覧回数
Vicky
Contributor I
Hi,
I have a requirement which is quite different which i never used earlier.
 
1. Declared a array in a file, test1.c
          unsigned int Store[10]; //Assume unsigned int takes 2 bytes of data
 
2. Now, I need to update store array with content of PC, SP, X, Y and other registers. //Assume, Store[] variable and copy logic would be in same file. I hope it should not be issue either
 
Question:
1. Is it possible to perform step2 above?
2. If its possible, can I have a short example for same.
 
Regards
Vicky
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,610件の閲覧回数
EmbeddedCoder
Contributor III
Hi Vicky,
 
It is certainly possible to grab the stack pointer content and store this in an Array via C.
 
I do something similar with the macro below:
 
ASM_STORE_STACK_PTR(pu8_stack);
 
Where the macro is defined as:
 
#define ASM_STORE_STACK_PTR(p_stack)   {__asm STS p_stack;}
 
you will need to check the S12 assembler manual, but there will be other assembler commands to grab the other registers.
 
Good luck!
0 件の賞賛
返信

2,610件の閲覧回数
EmbeddedCoder
Contributor III
I looked this up for you:
 
STAA will store the Acc A Reg
STAB will store the Acc B Reg
STX will store the Index X Reg
STY will store the Index Y Reg
 
so you can create other macros to store these values for you, as shown below:
 
#define ASM_STORE_ACC_A(p_acc_a)   {__asm STAA p_acc_a;}
#define ASM_STORE_ACC_B(p_acc_b)   {__asm STAB p_acc_b;}
#define ASM_STORE_IX_X(p_x)   {__asm STX p_x;}
#define ASM_STORE_IX_Y(p_y)   {__asm STY p_y;}
 
I'm not sure what storing the program counter will do for you as it will be the address of the place where you store the values?
Do you mean you want to store the program counter contained on the stack (i.e. the calling function)?
0 件の賞賛
返信

2,610件の閲覧回数
Xbot
Contributor II
0 件の賞賛
返信