mc9s12dt256 serial comm issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mc9s12dt256 serial comm issue

4,094 Views
Franklin
Contributor I
Hi,
 
I am trying to control another device with my hcs12 microcontroller using the serial port. The command I wish to send to the other device is
 
"P BE 2"    followed by the return key
 
Using hyperterminal, I can send this command and the device responds as expected. However, when I programmed my hcs12 to send the following code,
 
            byte RequestMsg[9] = {'P',' ','B','E',' ','2','\r','\n',0};
 
using the SendBlock, the other device does not respond.  I have tried using only a carriage return, only a line feed, and various other ascii symbols, to no avail. When I send the block to hyperterminal, the output is predictably, "P BE 2" 
 
Any ideas about the source of my problem are greatly appreciated
Labels (1)
0 Kudos
Reply
4 Replies

2,287 Views
nikosxan
Contributor I
Hello
 
First i think you should be sure that data goes to the device from you S12, so verify correct S12-Tx Device-Rx path at least, and Usually you DO need a null modem cable. Is there a way to verify data from S12 received by the device ? (for eg plot them to som kind of screen...). On last i would also analyse the behavior of car. return as understood by the device. Last but not least, exact match of comm settings....Does the device needs parity ???
0 Kudos
Reply

2,287 Views
bigmac
Specialist III
Hello,
 
You say that Hyperterminal will successfully communicate with the remote device.  Assuming you are using a "straight-through" cable, and since Hyperterminal will be operating as a DTE (data terminal equipment), this would mean that the remote device is configured as DCE (data communications equipment).
 
You also say that the HCS12 board can successfully communicate with Hyperterminal, and this implies that the board is currently configured as DCE.  Unless you can change the board configuration to DTE, you will need to use a null modem (cross-over) cable.
 
Regards,
Mac
 
0 Kudos
Reply

2,287 Views
Franklin
Contributor I
I was using the wrong cable. Thanks guys :smileyhappy: One of those knuckle-head mistakes, like trying forgetting to plug something in and wondering why it's not working... heh
0 Kudos
Reply

2,287 Views
JimDon
Senior Contributor III
Are you sure that you don't need a null modem cable to connect the board to the device?

If the are both DTE's the this could be the case.
0 Kudos
Reply